AXIS#.GEAR.DEC

Description

AXIS#GEAR.DEC defines the maximum deceleration rate the slave follows to come out of gearing, to rest. AXIS#GEAR.DEC is only be used if Gearing is stopped for any reason, including if an AXIS#.STOP command is issued. When the axis comes to rest, AXIS#GEAR.DEC is no longer in effect and the axis behaves according to the rules of the motion commanded next.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.GEAR.DEC

5006h

02h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.GEAR.DEC

5106h

02h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.GEAR.DEC

5501

157D

Unsigned32

Read/Write

Acceleration

AXIS2.GEAR.DEC

71037

1157

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.GEAR.DEC

5501

Float

Read/Write

Acceleration

Name

ID

Hex

Data Type

Access

AXIS#.GEAR.DEC

5501

157D

Unsigned32

Read/Write

Variants Supported

All variants are supported